June 16, 2020 by Bruce Rose - 7 Minute Read
In some applications the use of a single power supply may not be sufficient to provide the power required by the load. The reasons for using multiple supplies may include redundant operation to improve reliability or increased output power. When providing combined power, care must be taken to ensure power is delivered in a balanced manner by all of the supplies.
Redundant power supplies are a topology where the outputs of multiple power supplies are connected to increase the reliability of the system but not to increase the power output. Redundant configurations are normally designed to draw output current from only the primary power supplies and to draw current from the back-up power supplies when a failure has occurred in one of the primary power supplies. Since drawing load current places stress on the components in a power supply, high reliability in the system is achieved when no current is drawn from the redundant supplies until there is an issue with one of the primary supplies.
A common topology employed to increase output power is to connect the outputs of two or more supplies in parallel. In this configuration each power supply delivers the required load voltage while connecting the supplies in parallel increases the available load current and thus the available load power.
This topology can be successfully implemented but there are many considerations to ensure the efficiency of the configuration. For parallel configurations, power supplies with internal circuits are preferred as the internal circuits will improve the efficiency of the current sharing. If the power supplies used in a current sharing application do not have internal sharing circuits then external methods, which may be less efficient, must be used.
The primary concern is how evenly the load current is shared between the power supplies. The load current distribution is dependent upon both the design of the power supplies and the design of the external circuit and conductors used to connect the outputs of the supplies in parallel. It is almost always the case that identical supplies are used when connecting them in parallel due to the challenges of efficiently configuring the power supplies. However it is possible to configure supplies in parallel with matching output voltages and non-matching maximum output currents.
A more detailed discussion regarding connecting power supplies in parallel can be found in our Current Sharing with Power Supplies technical paper.
Another option to obtain greater power delivered to a load is to connect the outputs of multiple power supplies in series rather than in parallel. Some of the advantages to employing a series topology include: near perfect utilization of power delivery between the supplies, no need for configuration or sharing circuits, and a tolerance to a large variety of application designs. As mentioned previously, when connecting the outputs of supplies in parallel each supply provides the required voltage and the load current is shared between the supplies. In comparison, when the outputs of power supplies are connected in series, each supply provides the required load current and the output voltage provided to the load will be the combination of the supplies in series.
It should be noted that when power supplies are configured with the outputs connected in series the supplies do not need to have similar output characteristics. The load current will be limited to the lowest load current capability of any of the supplies in the configuration and the load voltage will be the sum of the output voltages of all of the supplies in the string.
There are a few limitations imposed upon the power supplies when they are used in a series output configuration. One of the limitations is that the output of the supplies must be designed to tolerate the voltage offset due to the series configuration. This offset voltage will normally not be an issue, but the output voltages of ground referenced power supplies cannot be stacked on the outputs of other supplies. A second limitation is that the output of a supply can be subjected to a reverse voltage if the output is not active when the remaining outputs in the string are active. The reverse voltage concern can be easily resolved by placing a reverse biased diode across the output of each supply. The breakdown voltage rating of the diode must be greater than the individual supply output voltage and the diode current rating must be greater than the highest output current rating of any power supply in the series string.
Power supplies connected in parallel:
Power supplies connected in series:
Although the common method employed to increase the load power delivered from power supplies is to connect the outputs in parallel another solution can be to connect the outputs of multiple power supplies is series. Power supply vendors such as CUI have technical staff who can help to configure an acceptable solution to these and other power supply application challenges.
Fundamentals , Product Selection
Have comments regarding this post or topics that you would like to see us cover in the future?
Send us an email at powerblog@cui.com