April 7, 2020 by CUI Inc -
5 Minute Read
Last updated September 19, 2023
When faced with the task of choosing an external power supply (EPS), it's important to consider several factors to ensure your application runs smoothly and efficiently. These include your system’s power requirements, package type, dc plug, efficiency and safety standards, EMI and EMC regulatory standards and customization options.
In this article, we will discuss the key considerations for selecting an external power supply and provide some tips on how to choose the right EPS for the specific needs of your design.
The first consideration when selecting a power supply is determining your system’s power requirements. Understanding the wattage, voltage, and amperage your system load requires is essential for the operation and safety of your end system. This includes asking questions like, “does my system operate at a constant power level and what are the minimum and peak power requirements?” If you are unsure or have questions, CUI Inc’s in-house engineering expertise can help.
2. Package Type – Desktop or Wall Plug?
External power supplies are generally offered in two package types: desktop or wall plug (fixed or multi-blade). For many applications either option will work. However, there are some reasons why you may select one over the other:
For an external adapter to power your design it needs a method of plugging into your system. If the receptacle or jack has already been selected, this will determine which dc plug you choose. One of the most common options is a 5.5 mm x 2.1 mm or “P5” dc barrel plug (5.5 mm OD, 2.1 mm ID, 9.5 mm L). CUI’s standard plug options include barrel plugs, USB, EIAJ, DIN, stripped and tinned, as well as locking and right angle options. If these don’t meet your needs, we can work with you to implement your own plug onto the adapter.
In addition to the dc plug, you’ll want to ensure the dc cord meets your needs. Is it long enough to reach your product? Does it have the desired appearance and pliability? It is important to understand that modifying the dc cord can impact both efficiency and safety regulations.
Making sure you’ve considered the end market where your system will be implemented is critical. Many countries have efficiency standards which regulate the amount of energy that may be ‘wasted’ by external power supplies. Whether it’s Level VI (US), CoC Tier 2 (EU), or ErP Lot 7 (EU) efficiency standards, CUI offers compliant models and can help you navigate the complex and dynamic regulatory landscape.
In addition to efficiency standards, it is imperative to make sure your adapter has the proper safety standards for the end application. For example, medical products need the 60601-1 certification and products for ICT/AV applications need the 62368-1 certification.
Many countries require agency marks which are unique to that country. Specialized design and testing are sometimes required to obtain these country-specific certifications. CUI has the experience and knowledge to work with you to meet your country-specific agency mark needs.
5. EMI and EMC
Many electronic products offered for sale are required to meet EMI and EMC (Electromagnetic Interference and Electromagnetic Compatibility) regulatory requirements. These requirements ensure that your product will not interfere with the proper operation of other products and similarly that the proper operation of your product will not be affected by other products. Although CUI external power supplies are certified to meet EMI and EMC regulatory standards, it is probable that your system (including the power supply) will also need to be tested and certified.
Another important consideration and question to ask is, “how well will the adapter aesthetically integrate with my system?” If your design has a desired look-and-feel and you care about the customer experience of your product, then don’t let the adapter be an afterthought. If your product has been intentionally designed with a specific color, then a black adapter may not integrate well. Consider color, texture, packaging, and even adding your logo to the power supply. CUI specializes in a range of customizable branding options.
Selecting a power supply for your new product is not a difficult task, but there may be subtle issues that affect the selection process. By working with an experienced power supply company, such as CUI, you can ensure that your power supply not only properly supports the operation of your product but also enhances the value of your product for your customer. CUI has a broad portfolio of standard designs we can customize to meet your specific application needs.
Have comments regarding this post or topics that you would like to see us cover in the future?
Send us an email at powerblog@cui.com