Table of Contents



PRODUCT SPOTLIGHT:
LOW POWER DC-DC CONVERTERS


Introduction

Welcome to the CUI Product Spotlight on low power dc-dc converters. Learn about selection criteria and design considerations for low power isolated dc-dc converters, including features and benefits followed by an introduction to CUI’s comprehensive line of 1~3 W products.

Objectives

  • Discuss selection criteria and design considerations for low power isolated dc-dc converters
  • Introduce CUI’s 1~3 W dc-dc converter family, including features, benefits, and key specifications

Criteria to Consider


There are a number of design criteria that an engineer must consider when selecting the appropriate low power dc-dc converter for their application. Aside from the general implementation of converting a dc input voltage to a dc output voltage, the engineer must understand the level of isolation required in the design, the tolerable voltage fluctuations that the architecture can withstand, and the types of protections that must be available. These variables, when combined with different packaging types, create a broad number of dc-dc converter options that an engineer must select from, including:

  • Inputs / outputs
  • Power conversion
  • Isolation
  • Regulation
  • Protections
  • Package

Input Voltage Requirements

The input of a dc-dc converter is tied to the output of an upstream supply in the power system. This will define the required input voltage necessary for the dc-dc converter. There are a number of different input options depending on the stability of the voltage. For example, a fixed input voltage can be used when the voltage rail connected to the input is very stable. If, on the other hand, the dc-dc converter is connected to a fluctuating supply, like a battery, then a much wider input range is required to account for the changing input voltage conditions. 2 to 1 and 4 to 1 type inputs are examples of wide input range devices used to address applications with a volatile input voltage. These numbers represent a comparison between the high and low input voltage limits. An example of a 2 to 1 input voltage device would be a dc-dc converter that has a nominal input of 12 volts but can operate anywhere between 9 volts and 18 volts while still maintaining a stable output voltage.

Available input ranges:

  • +/-10%
  • 2:1
  • 4:1

Fixed Output


The required output voltage is one of the easier decisions an engineer must make. The decision on the output voltage will be driven by the load requirements and whether the engineer wants to drive a single load or two loads.

Output voltage considerations:

  • Single / Dual
  • Positive / Negative

Power Conversion

A dc-dc converter can be used to step down a voltage, step up a voltage, or even invert a voltage from positive to negative. Which of these solutions is selected will depend on the type of load being driven and the power architecture of the design. The most common application is to step down the dc voltage from a higher voltage to a lower voltage. A distributed power architecture is an example of a power system that steps down dc voltages to create a series of voltage rails that drive different loads.

Step Down




Step Up




Inversion

Isolation


Dc-dc converters can be implemented to provide isolation in a system. This electrical separation creates a barrier which can be used for safety protection or noise isolation. Two isolation factors are generally specified: isolation resistance and isolation voltage. The isolation resistance is a function of the material and spacing employed in the dc-dc converter. The isolation voltage is defined as the maximum voltage across the isolation barrier that a device can withstand for a fixed time period. The actual breakdown voltage is typically in excess of 1000 volts higher than the rated isolation voltage. The reason for rating a conservative isolation voltage is to ensure that the isolation testing of a supply does not degrade the isolation barrier in any way. The required isolation voltage will depend on the market the device is being used in. Industrial applications will typically accept 1 kilovolt of isolation where as medical applications may require up to 6 kilovolts of isolation. The higher isolation required in medical applications is implemented in order to comply with restrictive standards mandated by agencies like UL and TUV.

Regulated vs. Non-Regulated

Another key parameter is regulation. Regulation is the ability of the dc-dc converter to maintain the output voltage within a specified range as input conditions change. There are two primary categories of dc-dc converters, regulated and non-regulated devices. Regulated dc-dc converters are used in applications where the input voltage is not well regulated. Fluctuations on the inputs will therefore not affect output voltages, thus driving subsequent downstream components. Non-regulated devices are used when the upstream signals are well regulated and line changes are minimal. The output voltages will fluctuate with changes in the line or the load. In general, non-regulated devices are generally smaller and less expensive than regulated dc-dc converters.

Regulated

  • Used where the input voltage is not well regulated
  • Outputs do not fluctuate with changes in line and load
  • Wide input range

Non-Regulated

  • Where the upstream signal is well regulated and fluctuations will be minimal
  • Outputs fluctuate with line and load changes
  • Narrow input range

Protections


  • Short Circuit
  • Over Voltage
  • Over Current / Over Load
  • Under Voltage

Output protections are implemented in dc-dc converters to prevent damage to the converter or attached loads. One type of protection is for short circuits. Short circuit protection kicks in and shuts down the device when a short circuit condition is created. Typically once the short is removed, the device will recover to normal operation. Over voltage protection similarly shuts down the dc-dc converter when its voltage exceeds a specified range. Over current or over load protection is a feature that limits the output current so the dc-dc converter will not be damaged. Finally, under voltage lock out is a protection where the device shuts downs when the input voltage drops below a certain level. Most dc-dc converters incorporate most if not all of these types of protections.

Applications

CUI’s low power dc-dc converters are designed with varying levels of isolation to address the needs for a range of industries and applications.

1 ~ 2 kVdc – Industrial, Telecom, Consumer Electronics

  • Industrial Controls
  • Wireless Sensing
  • Gaming
  • Ethernet Switches

3 kVdc – Medical

  • Imaging
  • Ultrasound
  • Home Diagnostics

6 kVdc – High Voltage Circuits

  • Laser
  • Mass Spectroscope
  • X-Ray Generator

Available Products

CUI's family of low power isolated dc-dc converters ranging from 1 W to 3 W are designed to provide an economical and reliable means of converting and/or isolating dc rails within a distributed power system. The units are housed in industry standard SIP, DIP or SMT packages and feature an ultra-wide operating temperature range from -40 up to +105°C, depending on the series. Available in regulated and unregulated versions, these lower power modules offer single and dual outputs, up to 4 to 1 input ranges, and isolation voltages up to 6000 Vdc. Designed to maximize efficiency at light and no load, this family is ideally suited for a variety of applications where energy consumption is a concern.

Highlights

  • 1 to 3 W power ratings
  • Industry standard SIP, DIP, and SMT packages
  • Regulated and unregulated models
  • Single and dual outputs
  • Up to 4:1 input ranges
  • Isolation voltages up to 6 kVdc
  • Ultra-wide temperature ranges from -40 up to 105°C
  • High efficiency at light load and no load
Unregulated - 1 W Unregulated - 2 W
Unregulated 1 W
Learn More
Unregulated 2 W
Learn More

Regulated - 2 W Regulated - 3 W View All Available 1 ~ 3 W Models
Regulated 2 W
Learn More
Regulated 3 W
Learn More
All 1 ~ 3 W
Learn More

Summary

There are a number of criteria to consider when selecting a dc-dc converter. These criteria include the required inputs, outputs, power conversion, isolation, regulation, protections, and packaging. Because of the wide variety of options, a vendor needs a broad line up to meet most customer needs. CUI’s extensive line of low wattage power supplies provides an engineer with multiple options.

 
Powered by Translations.com GlobalLink OneLink SoftwarePowered By OneLink